How to use the kpp for imx6q+android4.3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use the kpp for imx6q+android4.3?

跳至解决方案
3,166 次查看
燕频姜
Contributor II

Hello,

I want to use 4 row,4 col on my board.I have activated the keypad driver in the kernel and configured the column and row keypads in the board file.

In the device filesystem is  the entry :

I: Bus=0019 Vendor=0000 Product=0000 Version=0000

N: Name="imx-keypad"

P: Phys=

S: Sysfs=/devices/platform/imx-keypad/input/input1

U: Uniq=

H: Handlers=event1

B: PROP=0

B: EV=100013

B: KEY=3 0 0 0 0 0 0 40000800 1680 0 78000000 10000ffe

B: MSC=10

the interrupts is:

114:          0          0          0          0       GIC  imx-keypad

But,when press then button,there is no interrupts on.

How to set clk? The BSP has not kpp clk.

keypad->clk = clk_get(&pdev->dev, "kpp");

Has somebody an idea what could be the reason?

THX

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,310 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

i.MX KPP is designed to interface with a keypad matrix with 2-point contact or 3-point contact keys. If your application requires a different configuration, you can reference (in Linux) Documentation/devicetree/bindings/input/imx-keypad.txt to add the keymap in kpp driver configuration.

Also can you add debug message in drivers/input/keyboard/imx_keypad.c to check whether kpp driver is correctly loaded.

Additionally, in Linux BSP, the KPP driver does not ready for wakeup (generating interrupts in Suspend mode). The attached patch (for BSP L3.0.35_12.10.02_GA) enables KPP key detection in suspend mode (i.MX6SL).

Regarding Android integration, you could check the KPP configuration on the init.rc file. Please take a look at the following thread:

Where to edit init.rc?


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,311 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

i.MX KPP is designed to interface with a keypad matrix with 2-point contact or 3-point contact keys. If your application requires a different configuration, you can reference (in Linux) Documentation/devicetree/bindings/input/imx-keypad.txt to add the keymap in kpp driver configuration.

Also can you add debug message in drivers/input/keyboard/imx_keypad.c to check whether kpp driver is correctly loaded.

Additionally, in Linux BSP, the KPP driver does not ready for wakeup (generating interrupts in Suspend mode). The attached patch (for BSP L3.0.35_12.10.02_GA) enables KPP key detection in suspend mode (i.MX6SL).

Regarding Android integration, you could check the KPP configuration on the init.rc file. Please take a look at the following thread:

Where to edit init.rc?


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,310 次查看
燕频姜
Contributor II

Hi,Carlos

Thanks for your answer,I have solved this problem.I just set the wrong keymap.

Your another advice is  also very useful to me.

Best regards!

YanpinJiang

0 项奖励
回复
2,310 次查看
hrushinale
Contributor III

Hi YanpinJiang,

                        Actually I am also trying the same thing in Linux bu I am confused  in driver, Should I make any modifications in driver? Can you please share your board file and the Keymap you set ? may it solve my problem

                                                                                                                                   Thanks in advance

                                                                                              

0 项奖励
回复
2,310 次查看
燕频姜
Contributor II

I sorry I have not seen your message.

0 项奖励
回复