How to use nxp pin config tool for pin multiplexing in imx8mplus in yocto project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use nxp pin config tool for pin multiplexing in imx8mplus in yocto project?

1,543 Views
vivek338
Contributor IV

Hi !

I need help on pin multiplexing using config tool and integrate in yocto project. I am working imx8mplus development board.

Please help!

0 Kudos
Reply
4 Replies

1,529 Views
florian_arndt
Senior Contributor I

Hello vivek,

so what is your specific question?

0 Kudos
Reply

1,522 Views
vivek338
Contributor IV
Hi !

I want to change pin functionality using config tool and add that dts to yocto project.
0 Kudos
Reply

1,489 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @vivek338 !
Thank you for contacting NXP Support!

As @florian_arndt mentioned, Config Tools helps to generate a customized device tree according to your necessities.

To compile your customized device tree you can follow the next instructions.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-Devshell-to-compile-device-tr...


Best Regards!
Chavira

0 Kudos
Reply

1,516 Views
florian_arndt
Senior Contributor I

Hello @vivek338,

just select the pin multiplexing you want to have via the "Pins Tool" and then export it via the menu. You can find some pictures in the appendix.

1) Configure your multiplexing by clicking on the specific pins in the CPU ball grid.

florian_arndt_0-1712217666003.png


2) Or configure your multiplexing via interface selection in the left column.

florian_arndt_1-1712217691703.png


3) Then export it.

florian_arndt_2-1712217711289.png


4) Choose what you want to export.

florian_arndt_3-1712217733675.png


5) Select your target directory.

florian_arndt_4-1712217787851.png



I hope this helps.

0 Kudos
Reply