How to use mxc_vpu_test for transcoding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use mxc_vpu_test for transcoding

3,286 Views
yanfengliu
Contributor III

I am using mxc_vpu_test from FSL Yocto 3.10.17 with a i.MX6Q device. I can do both encode and decode correctly using "-E" and "-D" options correctly.

However, the transcoder function (-T)  seems not easy to use. Is there a working sample cmd line to transcode an input .mp4 file to a .264 output file using "-T" option of the mxc_vpu_test program?

Below is my usage on a headless i.MX6Q device, it doesn't work:

yf@imx6x-std:~/test$ ./mxc_vpu_test.out -T "-i akiyo.mp4  -o /tmp/akiyo.264"

[INFO] VPU test program built on Apr  2 2016 08:16:20

[INFO] Product Info: i.MX6Q/D/S

[INFO] VPU firmware version: 3.1.1_r46056

[INFO] VPU library version: 5.4.23

[INFO] Format: STD_MPEG4

[INFO] MPEG4 class: MPEG4

[INFO] Input file "akiyo.mp4" opened.

[INFO] Output file "/tmp/akiyo.264" opened.

[INFO] bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

[INFO] Mpeg4 Profile: 0 Level: 3 Interlaced: 0

[INFO] Aspect Ratio Table index: 1

[INFO] Decoder: width = 176, height = 144, frameRateRes = 15, frameRateDiv = 4294967295, count = 4

[INFO] CROP left/top/right/bottom 0 0 0 0

[INFO] v4l output to /dev/video17

[INFO] Display to 640 640, top offset 0, left offset 0

[INFO] Display: NV12

[INFO] Display fps will be 30

[INFO] Capture/Encode fps will be 30

[ERR] Encoder open failed -3

Guess my usage is incorrect for "-T" option. The Encoder open failure "-3" means invalid parameter but I don't know where the problem is according to the command line help.

Labels (3)
0 Kudos
Reply
3 Replies

2,712 Views
igorpadykov
NXP Employee
NXP Employee

Hi Janfeng

only video codec can be transcoded, not image.

example can be found on p.52 presentation :

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,712 Views
yanfengliu
Contributor III

Igor,

Thank you for the pointers. I retried with the "akiyo.mp4" and found it still doesn't work --- I copied the runtime log above.

The samples on p.52 of the slides just used a different input file:

/unit_tests/mxc_vpu_test.out -T "-i /home/linaro/mount_sd/Coral_Reef_Adventure_720_video.wmv3 -f 3 -t 1 -x 0 -y 0 -a 60 -w 1280 -h 720 -o /dev/shm/transcode.264 -q 25 -g 30"

It seems not working here either:

yf@imx6x-std:~/test$ ./mxc_vpu_test.out -T "-i akiyo.mp4 -f 0 -t 1 -x 0 -y 0 -a 60 -

o /tmp/akiyo.264 -q 25 -g 30"

[INFO] VPU test program built on Apr  2 2016 08:16:20

[INFO] Product Info: i.MX6Q/D/S

[INFO] VPU firmware version: 3.1.1_r46056

[INFO] VPU library version: 5.4.23

[INFO] Display through V4L2

[INFO] Format: STD_MPEG4

[INFO] MPEG4 class: MPEG4

[INFO] Input file "akiyo.mp4" opened.

[INFO] Output file "/tmp/akiyo.264" opened.

[INFO] bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

[INFO] Mpeg4 Profile: 0 Level: 3 Interlaced: 0

[INFO] Aspect Ratio Table index: 1

[INFO] Decoder: width = 176, height = 144, frameRateRes = 15, frameRateDiv = 4294967295, count = 4

[INFO] CROP left/top/right/bottom 0 0 0 0

[INFO] v4l output to /dev/video17

[INFO] Display to 640 640, top offset 0, left offset 0

[INFO] Display: NV12

[INFO] Display fps will be 60

[INFO] Capture/Encode fps will be 60

[ERR] Encoder open failed -3

Regards,

yanfeng

0 Kudos
Reply

2,712 Views
jack_mao
NXP Employee
NXP Employee

akiyo.mp4 is not a standard mp4 file

0 Kudos
Reply