How to use i.MX6ULL USB OTG Port to be Ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use i.MX6ULL USB OTG Port to be Ethernet

791件の閲覧回数
stevenyu
Contributor III

Hi Support,

We want to connect USB OTG port to Windows PC, and it may need CDC Ether built in.

Windows PC----usb line----USB OTG port of i.MX6ULL EVK

We have checked default menuconfig and found "Device Drivers->USB support->USB Modem (CDC ACM) support" is set to <M> by default already. 

Then, we connect USB OTG port to Windows PC, but we don't see anything happen on both sides. 

root@imx6ull14x14evk:~# ls -al /sys/bus/usb/devices/
1-0:1.0/ usb1/

Regards,

Steven Yu

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

585件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi Steven,

If the config is <M>, you have to copy the .ko file. And initialize after after booting using insmod command.

Regards,

Aravinth

0 件の賞賛
返信

585件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Steven

please check FSL-UT-USB-005-Gadget-Ethernet  test in imx-test

package (folder mxc_usb_test)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信