How to use i.MX6ULL USB OTG Port to be Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use i.MX6ULL USB OTG Port to be Ethernet

746 Views
stevenyu
Contributor III

Hi Support,

We want to connect USB OTG port to Windows PC, and it may need CDC Ether built in.

Windows PC----usb line----USB OTG port of i.MX6ULL EVK

We have checked default menuconfig and found "Device Drivers->USB support->USB Modem (CDC ACM) support" is set to <M> by default already. 

Then, we connect USB OTG port to Windows PC, but we don't see anything happen on both sides. 

root@imx6ull14x14evk:~# ls -al /sys/bus/usb/devices/
1-0:1.0/ usb1/

Regards,

Steven Yu

Labels (1)
0 Kudos
Reply
2 Replies

540 Views
aravinthkumarja
Senior Contributor II

Hi Steven,

If the config is <M>, you have to copy the .ko file. And initialize after after booting using insmod command.

Regards,

Aravinth

0 Kudos
Reply

540 Views
igorpadykov
NXP Employee
NXP Employee

Hi Steven

please check FSL-UT-USB-005-Gadget-Ethernet  test in imx-test

package (folder mxc_usb_test)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply