Hi Support,
We want to connect USB OTG port to Windows PC, and it may need CDC Ether built in.
Windows PC----usb line----USB OTG port of i.MX6ULL EVK
We have checked default menuconfig and found "Device Drivers->USB support->USB Modem (CDC ACM) support" is set to <M> by default already.
Then, we connect USB OTG port to Windows PC, but we don't see anything happen on both sides.
root@imx6ull14x14evk:~# ls -al /sys/bus/usb/devices/
1-0:1.0/ usb1/
Regards,
Steven Yu
Hi Steven,
If the config is <M>, you have to copy the .ko file. And initialize after after booting using insmod command.
Regards,
Aravinth
Hi Steven
please check FSL-UT-USB-005-Gadget-Ethernet test in imx-test
package (folder mxc_usb_test)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------