How to use freescale IO Mux tool output files in LTIB to support a custom design (ex. add new pads)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use freescale IO Mux tool output files in LTIB to support a custom design (ex. add new pads)?

1,545 次查看
YamilGarcia
Contributor III

I would like to change some pads configuration and add new pads to a custom design based on sabrelite board. I'm using freescale IO Mux tool to configure pads according to my needs. I've read the user manual for IO Mux tool but I couldn't figure out how to integrate IO mux tool's output file to LTIB in order to build the kernel.

I've checked every supported platform in LTIB and I couldn't see the output files format generated by IO Mux tool.

Can someone give a hint on this matter?

How to integrate IO Mux tool's output files into LTIB to build a kernel?

0 项奖励
回复
2 回复数

1,184 次查看
Yuri
NXP Employee
NXP Employee

I am afraid, the IOMUX tool's output is not intended for simple / automatic embedding into Linux building systems as LTIB.
The IOMUX can provide source examples, which may be used for manual correction of driver's sources. 

0 项奖励
回复

1,184 次查看
YamilGarcia
Contributor III

Thanks Yuri, that's what I thought.

0 项奖励
回复