How to use ddr tools to configure 3GDDR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use ddr tools to configure 3GDDR

1,038 次查看
coindu
Contributor IV

Hi ALL:

            I have ever used ddr tools to generate 1G and 2GDDR configure file ddr_init.c and ddrphy_train.c for I.MX8M and works well.   

           Now I need to configure 3GDDR file ,the ddr tool will calibration and gen code success . but when i make a new imx-boot and burn it into the SD card , it will stuck in kernel stage . the only difference is the DDR size, so, I think the ddr_init.c and ddrphy_train.c may error.

pastedImage_1.png

pastedImage_2.png

Is there a problem with my configuration?

i will modify follow files on uboot when modify DDR size

board\freescale\imx8mq_evk\ddr\ddr_init.c

board\freescale\imx8mq_evk\ddr\ddrphy_train.c

include\configs\imx8mq_evk.h   PHYS_SDRAM_SIZE

标签 (1)
0 项奖励
回复
1 回复

944 次查看
jamesbone
NXP TechSupport
NXP TechSupport

We have in place a document that explains how to use the DDR tool, and we have an excel file that help you to select the proper values regarding your memory, here is the link:  i.MX8 MSCALE SERIES DDR Tool Release (V2.10) 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复