How to use blob enc/blob dec U-Boot command.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use blob enc/blob dec U-Boot command.

6,539 Views
jdepedro
Contributor IV


Hi, I am trying to use the blob enc / blob dec command available in the U-Boot source code provided by NXP on my i.MX6Q module. However, I obtain the follownig output:

=> mw.b 14000000 0 16                         

=> md.b 14000000 16                           

14000000: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

14000010: 00 00 00 00 00 00                                  ......

=> blob enc $loadaddr 0x12001000 32 0x14000000

Encapsulating data to form blob

b080000a

4000010

14000000

f0400000

12000000

32

f8400000

12001000

62

870d0000

0

0

0

0

Error in Encapsulation -3

=>

Could you explain why this error happens? Could you provide an example of this command usage which should work?

Thanks

Tags (2)
8 Replies

5,788 Views
igorpadykov
NXP Employee
NXP Employee

Hi jdepedro

what  uboot version is used in the case, nxp uboot-imx ?

For enabling uboot security functions one can look at configurations

descibed in

uboot-imx.git - Freescale i.MX u-boot Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,788 Views
jdepedro
Contributor IV

Hi igorpadykov,

thanks for your quick answer!

Yes, I am using the last NXP U-Boot release based on v2015.04 for i.MX6Q. I have enabled all the configuration options that you said:

CONFIG_SECURE_BOOT
CONFIG_SYS_FSL_SEC_COMPAT 4 /* HAB version */
CONFIG_FSL_CAAM
CONFIG_CMD_DEKBLOB

CONFIG_SYS_FSL_LE

and also

CONFIG_CMD_BLOB

which is needed in order to enable the blob command.

Could you confirm whether the usage example that I give is correct, and whether there is any error in the job descriptor which appears written? Thanks

Edit: by the way, just in case it helps to discard other problems, I have been successful using signed and signed + encrypted U-Boot images.

0 Kudos
Reply

5,788 Views
giuliodominutti
Contributor III

I have the same problem, have you found a solution?

Thanks

0 Kudos
Reply

5,788 Views
BiyongSUN
NXP Employee
NXP Employee

5,788 Views
giuliodominutti
Contributor III

I used this guide with success with a linux kernel 3.15, now I upgraded to 4.1.15, and when it's enabled "Freescale CAAM-Multicore driver backend", the kernel has no errors, but at runtime it doesn't start, it freeze after a while. There are known issue on such a problem?

0 Kudos
Reply

5,788 Views
jdepedro
Contributor IV

I had a similar problem and it was some register access during caam probe. Moving some clock enabling solve it for me.

0 Kudos
Reply

5,788 Views
BiyongSUN
NXP Employee
NXP Employee

Actually we verify on the 4.1.15.  Please make sure you are using NXP official BSP.

If you are not using NXP reference, please check the system desgin including software and hardware. CMA size maybe need to be changed for your hardware.

BTW, NXP never release BSP with Linux kernel 3.15.

0 Kudos
Reply

5,788 Views
igorpadykov
NXP Employee
NXP Employee

Hi jdepedro

please create service request for providing additional

documentation for this case.

Best regards

igor

0 Kudos
Reply