How to use USB-4G module in imx8qxpmek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use USB-4G module in imx8qxpmek

1,122 Views
chenchen_xi
Contributor II

Hi, there.

I'm using the imx8qxpmek and I connect it with a USB-4G module manufactured by HUAWEI.

when the stick connect to the board, shows:

[ 2597.882269] usb 1-1: new high-speed USB device number 3 using cdns-usb3
[ 2598.042076] cdc_ether 1-1:2.0 wwan0: register 'cdc_ether' at usb-xhci-cdns3-1, Mobile Broadband Network Device, 02:1e:10:1f:XX:XX

i want to know how to dial and connect the Internet using the usb-4G module and use this module to access the Internet.

0 Kudos
Reply
1 Reply

942 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xi

one can try to use it in the same way as with i.MX6 on below link

port telephony on i.MX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply