How to use Serial Flash Memory (imx6ull)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use Serial Flash Memory (imx6ull)

2,811 次查看
hanikun
Contributor I

Sorry poor english. I need help or some hint.

I use I.mx6ull (var-dart-custom? from DART-6UL - Variscite Wiki )

and I should use IS25LP016D (It's serial flash memory http://www.issi.com/WW/pdf/25LP-WP016D.pdf )

I'm poor about linux build or device tree set.

but I found about SPI(DART-6UL SPI - Variscite Wiki )

//example.

&ecspi1 {
  fsl,spi-num-chipselects = <1>;
  cs-gpios = <&gpio4 26 0>;
  pinctrl-names = "default";
  pinctrl-0 = <&pinctrl_ecspi1_1>;
  status = "okay";
          chip1: spidev@0 {
                compatible = "spidev";
                spi-max-frequency = <12000000>;
                reg = <0>;
         };
 };
&iomuxc {
  //imx6ul-evk {
   pinctrl_ecspi1_1: ecspi1grp {
    fsl,pins = <
     MX6UL_PAD_CSI_DATA07__ECSPI1_MISO       0x100b1 
    MX6UL_PAD_CSI_DATA06__ECSPI1_MOSI       0x100b1 
    MX6UL_PAD_CSI_DATA04__ECSPI1_SCLK       0x100b1
     MX6UL_PAD_CSI_DATA05__GPIO4_IO26        0x100b1
    >;
   };
  //};
 };
but I use spidev by python. but It looks like doesn't work. I use spidev's method like 
(readbytes, writebytes, xfer) all of them return just [0]. 
actually, I want to this one [IS25LP016D] to flash disk. like just mount. 
what should I do? I found like this.
//m25p80 is like a common spi flash driver.?
&ecspi1 {    pinctrl-names = "default";    pinctrl-0 = <&pinctrl_ecspi1_1>;     status = "okay";     cs-gpios = <&gpio4 24 0>;     flash@0 {        compatible = "m25p80", "jedec,spi-nor";        spi-max-frequency = <20000000>;        reg = <0>;     }; };
&iomuxc ・・・・
         pinctrl_ecspi1_1: ecspi1grp {
                 fsl,pins = <
                         MX6UL_PAD_CSI_DATA07__ECSPI1_MISO       0x100b1
                         MX6UL_PAD_CSI_DATA06__ECSPI1_MOSI       0x100b1
                         MX6UL_PAD_CSI_DATA04__ECSPI1_SCLK       0x100b1
                 >;
         };
but It's error like this. sorry about poor skill.
m25p80 spi0.0: unrecognized JEDEC id bytes: 9d, 60, 15
I found spi-nor / mtd / something else. but I need more helpful info or some advise or uage example. thanks.
标签 (2)
0 项奖励
回复
2 回复数

2,606 次查看
igorpadykov
NXP Employee
NXP Employee

Hi seunghan

for this memory one can look at patch

[4.14,107/143] mtd: spi-nor: Add support for is25wp series chips - Patchwork 

and use sect.3.8 SPI NOR Flash Memory Technology Device (MTD) attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,606 次查看
hanikun
Contributor I

I finally soved problem. and thanks about comments. It's good hint.

0 项奖励
回复