How to use STC_RIL_SetInterleave function in SCFW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use STC_RIL_SetInterleave function in SCFW

2,337 Views
luozhu
Contributor I

My board is imx8qm-mek,It has two DDRC.I found that the default interleaving size for A-core CPUs accessing DDR memory is 4KB. That is, the first 4KB is accessed through DDRC0 and the second 4KB is accessed through DDRC1. I want to change this size to 8KB. I found that the STC_RIL_SetInterleave function in the SCFW seems to achieve my requirement. I called STC_RIL_SetInterleave(STC10, kSTC_Interleave8K); in the board_init_ddr function, but it didn't work. Can you help me understand how to use this function?

0 Kudos
Reply
4 Replies

2,282 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @luozhu 

 

The STC_RIL_SetInterleave function is used in build_mx8qm_b0/soc/MX8QM/soc.o, the soc.c it's not open source. We don't recommend you modify it. If you still need to modify it. You can use like this.

 

STC_Type *bases[] = STC_BASE_PTRS;

 

for(int i; i < STC_count; i ++)

{

STC_Type *base = bases[i]

STC_RIL_SetInterleave(base,  <your stc config>)

}

 

0 Kudos
Reply

2,043 Views
wangbo9105
Contributor II

Hi,@Zhiming_Liu

The code I wrote are as you described. 


I have found an issue:

The function board_qos_config() normally won't be entered unless ss_updown_db(SC_PGP_XXX, 0x1); is called.

(1) I speculate that the implementation of STC_RIL_SetInterleave is as follows:

void STC_RIL_SetInterleave(STC_Type *base, stc_interleave_mode_t interleave)
{
if (base == NULL ) {
return;
}

interleave &= 0x3;
base->INTERLEAVE_SEL = interleave;
}

After I used your code to disable the memory interleaving mode for 16 STC instances, I read the value of base->INTERLEAVE_SEL. Only subsystem 15 (base->INTERLEAVE_SEL=0x3) was set successfully. For the other subsystems, base->INTERLEAVE_SEL=0x0 failed to set, but base->RVSD_HPR_ENABLE=0x3. I don't know why it was set to RVSD_HPR_ENABLE. What is the relationship between INTERLEAVE_SEL and RVSD_HPR_ENABLE?

Could you please provide a manual describing the STC registers?

(2) When entering the board_qos_config(sc_sub_t ss) function, the value of ss is always 15. Does this mean only subsystem 15 can reconfigure the memory interleaving mode?

I am eagerly looking forward to your response!

0 Kudos
Reply

2,069 Views
wangbo9105
Contributor II

Hi,@Zhiming_Liu

I also have a similar problem on the IMX8 board. I want to disable the memory interleaving mode.

How can I modify it in the source code? I don't know where to modify to make it work?

My question link is as follows:

https://community.nxp.com/t5/i-MX-Processors/How-to-modify-or-disable-the-memory-interleaving-access...

Looking forward to your reply

0 Kudos
Reply

2,270 Views
luozhu
Contributor I

@Zhiming_Liu 

Thanks,but where can i do this in src/scfw_export_mx8qm_b0/platform/board/mx8qm_mek/board.c file?

0 Kudos
Reply