How to use PN532 module to iMX8M Plus EVK via UART3?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use PN532 module to iMX8M Plus EVK via UART3?

2,157 次查看
NealZhang
Contributor III

Hi all,

I am trying to testing a PN532 module. This module support to connect to core board with I2C, SPI, HSU. I connect this module with UART3 on iMX8M Plus EVK board(EXP_CN PIN 8/10). But I cannot get any info with stty or minicom. BTW, I get nothing when i shot pin-8 and pin-10

I did not update image in the EMMC

Someone could have some advice?

image.png

0 项奖励
回复
9 回复数

2,131 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You need align the software for the UART3

0 项奖励
回复

2,113 次查看
NealZhang
Contributor III
You mean I need to modify the DTS file, and recompile the image to enable UART3?

2,067 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you are right.

0 项奖励
回复

2,052 次查看
NealZhang
Contributor III

Sry Sir,

I check the dts file of imx8mp-evk, and the uart is set as below

NealZhang_0-1724235494614.png

However, I cannot get anything with connecting the pin of UART3_TX and UART3_RX

Is there any other problems?

Thank u very much.

0 项奖励
回复

2,014 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @NealZhang ,

I help create new case 00645499  to our NFC team, our engineer will support you there by email.

Any questions contact us freely.

Wish you have a nice day

Best Regards

Rita

0 项奖励
回复

1,943 次查看
NealZhang
Contributor III

Hi, Rita Wang,

Could you please let me know if the PN7160 can be used with the libnfc-nci library? I read AN11697, which is a guide for using libnfc-nci with PN7120 and PN7150. However, I couldn't find any information indicating that this library supports the PN7160.

NealZhang_1-1724753322960.png

 

In addition, if the kernel driver nxp-pn5xx also supports PN7160 or not?

NealZhang_2-1724753362555.png

 

By the way, I'm going to integrate a NFC module into a linux board based on I.MX 8MPLUS, and we plan to use PN7160 for the advice from NXP official website

NealZhang_0-1724753289267.png

 

0 项奖励
回复

1,922 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @NealZhang

I already ask our NFC engineer Daniel help it in the new case 00645499, he will follow you and update to there, you can check in the email when he give update.

Wish you have a nice day

Best Regards

Rita

0 项奖励
回复

1,947 次查看
NealZhang
Contributor III
Sry,Could you please info me how to get into the case and the email address that I can query some problems via it?
0 项奖励
回复

1,958 次查看
NealZhang
Contributor III

Thank you very much

0 项奖励
回复