How to use PN532 module to iMX8M Plus EVK via UART3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use PN532 module to iMX8M Plus EVK via UART3?

2,376 Views
NealZhang
Contributor III

Hi all,

I am trying to testing a PN532 module. This module support to connect to core board with I2C, SPI, HSU. I connect this module with UART3 on iMX8M Plus EVK board(EXP_CN PIN 8/10). But I cannot get any info with stty or minicom. BTW, I get nothing when i shot pin-8 and pin-10

I did not update image in the EMMC

Someone could have some advice?

image.png

0 Kudos
Reply
9 Replies

2,350 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You need align the software for the UART3

0 Kudos
Reply

2,332 Views
NealZhang
Contributor III
You mean I need to modify the DTS file, and recompile the image to enable UART3?

2,286 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you are right.

0 Kudos
Reply

2,271 Views
NealZhang
Contributor III

Sry Sir,

I check the dts file of imx8mp-evk, and the uart is set as below

NealZhang_0-1724235494614.png

However, I cannot get anything with connecting the pin of UART3_TX and UART3_RX

Is there any other problems?

Thank u very much.

0 Kudos
Reply

2,233 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @NealZhang ,

I help create new case 00645499  to our NFC team, our engineer will support you there by email.

Any questions contact us freely.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply

2,162 Views
NealZhang
Contributor III

Hi, Rita Wang,

Could you please let me know if the PN7160 can be used with the libnfc-nci library? I read AN11697, which is a guide for using libnfc-nci with PN7120 and PN7150. However, I couldn't find any information indicating that this library supports the PN7160.

NealZhang_1-1724753322960.png

 

In addition, if the kernel driver nxp-pn5xx also supports PN7160 or not?

NealZhang_2-1724753362555.png

 

By the way, I'm going to integrate a NFC module into a linux board based on I.MX 8MPLUS, and we plan to use PN7160 for the advice from NXP official website

NealZhang_0-1724753289267.png

 

0 Kudos
Reply

2,141 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @NealZhang

I already ask our NFC engineer Daniel help it in the new case 00645499, he will follow you and update to there, you can check in the email when he give update.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply

2,166 Views
NealZhang
Contributor III
Sry,Could you please info me how to get into the case and the email address that I can query some problems via it?
0 Kudos
Reply

2,177 Views
NealZhang
Contributor III

Thank you very much

0 Kudos
Reply