How to use FreeRTOS_BSP_1.0.0_iMX6SX in code warriors IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use FreeRTOS_BSP_1.0.0_iMX6SX in code warriors IDE

跳至解决方案
1,480 次查看
chandiniindavar
Contributor IV

Hi,

I have downloaded FreeRTOS_BSP_1.0.0_iMX6SX  setup for imx6sx and used mx6sx_sdb_m4 demo app..

FreeRTOS_BSP_1.0.0_iMX6SX  supports 3 IDES  that is ARM GCC, iAR , DS-5 . but i looking for CODE WARRIORS.

Is nxp has supported setup for this IDE AS WELL ?

If not how to port this FREERTOS BSP to code warriors ?

Could any one guide me please ?

Thanks in advance

Chandini

标签 (2)
1 解答
1,244 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chandini

unfortunately CodeWarrior does not support i.MX platforms,

supported platforms are provided on

CodeWarrior Development Studios|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,245 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Chandini

unfortunately CodeWarrior does not support i.MX platforms,

supported platforms are provided on

CodeWarrior Development Studios|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,244 次查看
chandiniindavar
Contributor IV

Thanks for your replay igor..

0 项奖励
回复