How to use FreeRTOS_BSP_1.0.0_iMX6SX in code warriors IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use FreeRTOS_BSP_1.0.0_iMX6SX in code warriors IDE

Jump to solution
1,494 Views
chandiniindavar
Contributor IV

Hi,

I have downloaded FreeRTOS_BSP_1.0.0_iMX6SX  setup for imx6sx and used mx6sx_sdb_m4 demo app..

FreeRTOS_BSP_1.0.0_iMX6SX  supports 3 IDES  that is ARM GCC, iAR , DS-5 . but i looking for CODE WARRIORS.

Is nxp has supported setup for this IDE AS WELL ?

If not how to port this FREERTOS BSP to code warriors ?

Could any one guide me please ?

Thanks in advance

Chandini

Labels (2)
1 Solution
1,258 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chandini

unfortunately CodeWarrior does not support i.MX platforms,

supported platforms are provided on

CodeWarrior Development Studios|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,259 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chandini

unfortunately CodeWarrior does not support i.MX platforms,

supported platforms are provided on

CodeWarrior Development Studios|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,258 Views
chandiniindavar
Contributor IV

Thanks for your replay igor..

0 Kudos
Reply