How to use Flexray to iMX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use Flexray to iMX6?

1,360 Views
wangben
Contributor I

Hi ,

I used iMX6 in my project, I want to use Flexray and choice MFR4310+ TJA1080, but MFR4310 is using Asynchronous Memory Interface.

How to connect MFR4310 to iMX6? If it can not to do, which the solution of Flexray is good?

B.R

Ben

0 Kudos
Reply
2 Replies

1,152 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Wang,

  The only way  that I see to interface it, it is using the  EIM interface, just like it shows the reference manual of the MFR4310 in the figure 2.7.  MPC Interface with MPC5xx and MPC5xxx Families.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,152 Views
wangben
Contributor I

Hi James,

Thanks! I will study it.

Ben

0 Kudos
Reply