How to use Flexbuild to flash Debian image into eMMC on i.MX8M Plus EVK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use Flexbuild to flash Debian image into eMMC on i.MX8M Plus EVK?

162 Views
Lin113
Contributor II

Hi all,

I’m working with the i.MX8M Plus EVK and using NXP’s Flexbuild system to generate Debian images.
So far I can build, customize, and flash the image to an SD card with flex-installer, and it boots fine.

Now I want to deploy the same Debian image into the on-board eMMC instead of booting from SD.
From the Flexbuild user guide I noticed that flex-installer mentions support for installing to “SD/eMMC card or USB/SATA disk,” but I couldn’t find a clear example or procedure for eMMC on the i.MX8M Plus EVK.

  • Is there an official workflow to flash the Debian image to eMMC using Flexbuild tools?

  • Do I need to manually handle bootloader + partitioning with U-Boot (mmc dev, mmc write) after preparing the rootfs, or is there a ready-made script for this?

  • In Yocto BSP we usually use uuu/imx-uuc to flash into eMMC, but I don’t see a similar flow for Debian Flexbuild. Is there one?

Any detailed steps or reference document would be appreciated.

Thanks.

0 Kudos
Reply
2 Replies

134 Views
Lin113
Contributor II

I solve it

129 Views
danielchen
NXP TechSupport
NXP TechSupport

flex-installer is used to deploy those images to eMMC.

0 Kudos
Reply