How to use Cortex-M4 in i.max8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use Cortex-M4 in i.max8

1,109 次查看
wenfu
Contributor III

We need to use the M4 core to hander some SPI peripheral. The question are:

1,How to setup de firmware development for M4 core?

2,How M4 communicate with A53 linux?

...

I'm a newbie on this, thank you for any helpfull message.

0 项奖励
回复
1 回复

1,030 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wen

one can look at RPMsg Chapter in Linux Manual and

sect.2.8.5 Running i.MX RPMsg Test Programs in

Linux 5.4.3_1.0.0 Documentation

For M4 please use MCUXpresso SDK, build it on

Welcome | MCUXpresso SDK Builder 

rpmsg\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复