How to use Config Tools for i.MX v7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use Config Tools for i.MX v7

1,636 Views
hiroki_c_hashim
Contributor I

Dear all

I have a question. Please tell me know.

In Config Tools for i.MX v7 , there are the following items.

pastedImage_2.png

Among these are "Reset" and "NoInit".

When should these be set?

Labels (1)
0 Kudos
Reply
3 Replies

1,528 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Hiroki Hashimoto,

I’m still waiting for further information on why these options have been added, but both “reset” and “Noinit” would result on the registers keeping their reset values.

I will let you know as soon as I have more information.

Regards,

0 Kudos
Reply

1,528 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Hiroki Hashimoto,

I received confirmation from our experts on how these options work:

In Config Tools for i.MX there is no difference in Pins tool generated code for "No init" and "Reset" in the pin configuration. No C code for modification is generated for these options.

However, this is true only when all electrical properties are displayed in italic (means after-reset). When anything is set to user-specified value (displayed as non-italic) then generated code may include setting also for other bit-fields of non-zero values for electrical properties configured in given register. This is how the code generation script handles pin routing for i.MX devices.

I hope this information helps!

Regards,

0 Kudos
Reply

1,528 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Hiroki Hashimoto,

The documentation has not much details on these options. I’m investigating and I’ll let you know as soon as I have more information.

Regards,

0 Kudos
Reply