How to use AppWizard with MCUXpresso?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use AppWizard with MCUXpresso?

2,920 Views
adj
Contributor I

Reading the documentation on AppWizard is seems to support easy integration to the Segger Embedded Studio. Since NXP licences the AppWizard I would like to use it with MCUXpresso. 

Can anyone help with a how to?

4 Replies

2,753 Views
guitardenver
Contributor IV

Here is a video of how to export the AppWizard files and modify the emWIN example you get with your SDK.

https://www.youtube.com/watch?v=rdNM0LGWxfw

2,754 Views
deepakrana
NXP Employee
NXP Employee

Refer community link: SEGGER AppWizard Enabling Advanced GUI Design i... | NXP Community

2,754 Views
adj
Contributor I

Thanks for your input. I'll give it a try when I'm at work.

rgs,

Alexander

0 Kudos
Reply

2,754 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Alexander,

Hope you are doing well.

At the moment, we do not have examples using AppWizard directly with MCUXpresso. The user guide states that it will generate C code that you can implement to an emwin example to get you started. 

The porting and modifications are to be done by the customer. 

Please refer to UM03003, section 5.1 UM03001.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply