How to use 2nd IPU unit on imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use 2nd IPU unit on imx6

ソリューションへジャンプ
2,547件の閲覧回数
DraganOstojic
Contributor V

I'm aware that there are 2 IPU units on imx6. How can I use 2nd IPU unit?

This is in general how I currently use IPU:

// open IPU

int fd_ipu = open("/dev/mxc_ipu", O_RDWR, 0);


// use IPU


...

ioctl(fd_ipu, ..., ...);


// close IPU

close(fd_ipu);


Can this code be extended to differentiate between accessing 1st or 2nd IPU unit?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,682件の閲覧回数
rogerio_silva
NXP Employee
NXP Employee

Hi Dragan,

Using the Linux IPU driver, it's not possible to specify what IPU will be used. The driver handles it automatically and assigns each task for the available IPU.

If you want to use both IPUs at the same time (e.g. to process a specific task faster using 2 IPUs), you can open /dev/mxc_ipu once, create 2 threads and call the iotcl to perform the operation you want inside each thread.

I tried this approach and it works.

Rgds

Rogerio

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,683件の閲覧回数
rogerio_silva
NXP Employee
NXP Employee

Hi Dragan,

Using the Linux IPU driver, it's not possible to specify what IPU will be used. The driver handles it automatically and assigns each task for the available IPU.

If you want to use both IPUs at the same time (e.g. to process a specific task faster using 2 IPUs), you can open /dev/mxc_ipu once, create 2 threads and call the iotcl to perform the operation you want inside each thread.

I tried this approach and it works.

Rgds

Rogerio

0 件の賞賛
返信
1,682件の閲覧回数
DraganOstojic
Contributor V

Hi Rogerio, that is a neat trick. I'll give it a try.

Thanks.

0 件の賞賛
返信