How to understand VDI path

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to understand VDI path

2,529件の閲覧回数
yafengge126
Contributor II

Qiang_FSL‌

您好,li-sir

关于patch,

iMX6 camera patch to support CSI->VDI->IC->MEM and CSI->VDI->MEM capture 

请问下面的路径代表什么含义?

--------------

1.) CSI->IC->MEM
2.) CSI->MEM

3.) CSI->VDI->IC->MEM
4.) CSI->VDI->MEM

--------------

另外,IC代指的是什么?谢谢!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,316件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

That is the camera video data path, you can find it in reference manual, the IC module can do resize and CSC:

01.jpg

0 件の賞賛
返信

2,316件の閲覧回数
yafengge126
Contributor II

understood, thank u!

0 件の賞賛
返信

2,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Steven

for understanding VDI may be useful presentation

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信