Hi @Harvey021 ,
I assume that the i.MX6UL custom board establishes no more than four connections, the idle connection would be closed after 90 seconds.
So, I try to modify two TCP variables below.
tcp_fin_timeout
path: kernel-source/include/net/tcp.h
change TCP_TIMEWAIT_LEN from (60*HZ) to (90*HZ)
tcp_max_orphans
path: kernel-source/net/ipv4/tcp.c
change sysctl_tcp_max_orphans from (cnt/2) to 4
However, the i.MX6UL custom board can still connect to more than four servers.
Which variables should be modified?
How to change the value to comply with the requirements?
Best Regards,
Tammy