How to tune LVDS clock at 74.25 MHz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to tune LVDS clock at 74.25 MHz

跳至解决方案
1,557 次查看
christophe
Contributor V

Hi,

We have a custom board working with an imx6Q and the 3.0.35 ltib version.

We have 2 displays: the first one is a 720x1280 lcd display, running at 74.25 MHz, and the secondth one is a 1280x720 lvds display.

In order to meet specifications, we need to output video on the lvds display with a clock of 74.25 MHz. Up to now, the lvds display uses pll2 at 528 MHz. Since in the clock path, this frequency is divided by 7 and has a multiplicator of 35/N applied, we can only have 528*35/(18*7) = 75.4 MHz or 528*35/(19*7) = 71,5 MHz. But not 74.25 MHz.

We have tried to use pll5 but without success (a 10 MHz clock is generated).

So our question is: is it possible to match a 74.25 MHz frequency on lvds output ? And if yes, by which mean ?

Best regards,

Christophe

标签 (2)
0 项奖励
回复
1 解答
1,323 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi

With changes on ldb, this may help:

https://community.nxp.com/message/642150 

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,324 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi

With changes on ldb, this may help:

https://community.nxp.com/message/642150 

Regards

0 项奖励
回复