How to test the interfaces over the IMX 6SX based target board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test the interfaces over the IMX 6SX based target board

1,388 Views
tomaszsliwinski
Contributor III

Hi Yuri,

I am trying to run one of the bare metal examples on NXP Sabre MCIMX6SX. 

I transfer sdk_unit_test_ALL.bin to SD card and try to boot.

I connect putty to both serial debug ports (one for M4, one for A9).

Nothing seems to happen.

Am I missing something?

thanks,

Tomasz

0 Kudos
Reply
2 Replies

1,212 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  The Platfrom SDK was intended for i.MX6 D/Q/S/SDL/SL. The i.MX 6SX was not

launched yet at the SDK creation times.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,212 Views
tomaszsliwinski
Contributor III

Understood, thank you.    

What would you recommend as a starting point for bare metal on A9 for i.mx 6sx?

So far we are using:

1) made some mods to u-boot code and run it off an SDcard successfully.

2) working on getting Ds-5+ulink pro D going.

thanks,

Tomasz

0 Kudos
Reply