How to test USB eye diagram on i.MX8M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test USB eye diagram on i.MX8M?

4,781 Views
charleshuang
Senior Contributor II

Hi , we want to test USB eye diagram on iMX8M

But we don't know how to test , we have already seen this link i.MX6Q/eye pattern of USB HS1 setup 

We have tried the register (DCTL)

#./memtool -32 0x3810c704=0x00F00008

but it's not work for us and evk board.

We want to force to output Test Packet , how to do this ?

thanks

Labels (1)
0 Kudos
Reply
7 Replies

4,484 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  I've sent You a preliminary document, hope it helps.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply

4,484 Views
jonas_blick
Contributor I

Hi Yuri, 

Im trying to do this as well, can you send me the document/patch also?

Thank you!

0 Kudos
Reply

4,484 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You message directly.

Regards,

Yuri.

0 Kudos
Reply

4,413 Views
ktim_chen
Contributor I

Hi Yuri,

I have the same question, could you send the document to me?

Thank you.

0 Kudos
Reply

4,408 Views
Yuri
NXP Employee
NXP Employee

@ktim_chen 
Hello,

   Use app note AN12409 (i.MX6/7/8 series USB Certification Guide)

https://www.nxp.com/docs/en/application-note/AN12409.pdf

 

Regards,
Yuri.

0 Kudos
Reply

3,542 Views
tsmt
Contributor II

Link is invalid, is it possible that NPX provides an i.MX8 series USB certification guide

0 Kudos
Reply

3,589 Views
mayqueen
Contributor IV

We're almost mass production but face USB eye diagram testing problems on IMX8MP/IMX8MM, and I check this link already invalided, could you provide a new link to me? Thanks a lot

0 Kudos
Reply