How to test IMX7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test IMX7?

1,492 Views
imx7newbie
Contributor II

Hi,

I am very new to IMX7/Yocto Linux.

I got a board having IMX7 from Phytec

phyBOARD-Zeta (i.MX 7) - Develop.phytec - PHYTEC Wiki 

 and loaded the prebuilt Image and found following output on terminal(see attachment).

After linux booted, it comes following

"random: nonblocking pool is initialized".

What is this?

When I plug LAN cable it comes:

"fec 30be0000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx        
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready "

Actually I have no idea how to test IMX7? Any Idea?

I would like to use its PCIE interface for a project.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,182 Views
igorpadykov
NXP Employee
NXP Employee

Hi

one can follow nxp linux documentation found on

i.MX Software|NXP 

FreeRTOS documentation on

i.MX 7Dual Arm Cortex-A7 Processor|NXP 

and application notes on

i.MX 7Dual Arm Cortex-A7 Processor|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply