How to switch bootlets/bootstream partition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to switch bootlets/bootstream partition

2,251件の閲覧回数
Gatts
Contributor I

As a part of of our remote upgrade procedure,I would like to flash and boot the target from a secondary partition (for ex: /dev/sdb7 instead of /dev/sdb2).
I modified the script to flash the bootlets in secondary partition i.e., /dev/sdb7 but not sure how to boot from the secondary partition.

Please let  me know if you've any pointers?. My fdisk is as follows:



/ltib$ sudo fdisk -lu /dev/sdb

Disk /dev/sdb: 7969 MB, 7969177600 bytes
246 heads, 62 sectors/track, 1020 cylinders, total 15564800 sectors
Units = sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x77826d86

   Device Boot      Start         End      Blocks   Id  System
/dev/sdb1              62      625331      312635    b  W95 FAT32
/dev/sdb2          625332      838859      106764   83  Linux (changed to linux partition for testing)
/dev/sdb3          838860     1464191      312666   83  Linux
/dev/sdb4         1464192    15557039     7046424    5  Extended
/dev/sdb5         1464254     2089523      312635   af  HFS / HFS+
/dev/sdb6         2089586     2714855      312635    b  W95 FAT32
/dev/sdb7         2714918     2928383      106733   53  OnTrack DM6 Aux3 (New Bootlet partition)
/dev/sdb8         2928446     3553715      312635   83  Linux
/dev/sdb9         3553778     4179047      312635   af  HFS / HFS+
/dev/sdb10        4179110     6238067     1029479   83  Linux
/dev/sdb11        6238130     6665123      213497   83  Linux
/dev/sdb12        6665186    15557039     4445927   83  Linu

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,136件の閲覧回数
YixingKong
Senior Contributor IV

Sunll

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,136件の閲覧回数
YixingKong
Senior Contributor IV

Sunll

We have not got your response yet and will close the diacussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,136件の閲覧回数
YixingKong
Senior Contributor IV

Sunil

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the

issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,

Yixing

0 件の賞賛
返信