How to support the nandflash on IMX258

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to support the nandflash on IMX258

2,326 Views
wangqinghao
Contributor I

nand:TC58NVG1S3

gcc:arm-elf-gcc 4.6.3

cygwin:

I have compiled the ATK source codes to generate mx25_nand.bin,then copy it to AdvancedToolKit-MAX(Flash Tool) which can operate the FALSH.when I click the button Erase,the Flash Tool show "Failed to initial flash or not support this Flash,please reset the target"

Because TC58NVG1S3 configuration has already in the source code nand_device_info.c,I think I would not do something.Please ,thankyou!

0 Kudos
Reply
6 Replies

2,218 Views
igorpadykov
NXP Employee
NXP Employee

Hi

yes it should work, one can attach jtag debugger and try to debug it.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,218 Views
wangqinghao
Contributor I

Is the CPU support general Jtag, like 8.0 or 9.0.Thankyou!

I can not find arm-elf-gcc4.1.1.exe on WEB,that the manual recommended .So I hope you could give me one.

0 Kudos
Reply

2,218 Views
wangqinghao
Contributor I

Thank you!

Could you give me a GCC version on arm-elf-gcc4.1.1.exe?

0 Kudos
Reply

2,218 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I sent You link to download the arm-elf-gcc via e-mail.

Regards,

Yuri.

0 Kudos
Reply

2,218 Views
wangqinghao
Contributor I

The gcc4.1.1 is ok!

thank you!

0 Kudos
Reply

2,218 Views
wangqinghao
Contributor I

It`s very very kind of you,thanks!!

0 Kudos
Reply