How to support I2S communicate in L4.1.15

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to support I2S communicate in L4.1.15

1,638 次查看
guochgz
Contributor III

Hello:

      on my board, Lmx2571 is connected to the IMX6ULL's sai3.

      pastedImage_1.png

   I have followed this post:

   i.MX7Dual + SGTL5000 no data on SAI output 

   to added simple-audio-card on my baseline, but after do that , there is nothing show on my board.

   pastedImage_4.png

   my dts file is like this:

   pastedImage_6.png

   pastedImage_7.png

   pastedImage_8.png

标签 (2)
0 项奖励
回复
2 回复数

1,560 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 国承 张

one can try "simple-audio-card" patch :

ARM: dts: imx6ul-14x14-evk: Add audio support - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,560 次查看
guochgz
Contributor III

thanks igor, I have solved this issue by add code in soc-util.c.

0 项奖励
回复