How to terminate unused ONOFF and PMIC_ON_REQ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to terminate unused ONOFF and PMIC_ON_REQ?

ソリューションへジャンプ
1,903件の閲覧回数
adevries
Contributor V

Hello,

My design will be powering the 8M Mini using an external PMIC, so I don't need to use the ONOFF signal or PMIC_ON_REQ signal provided on the 8M Mini. How should these signals be terminated when they are unused?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,782件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi adevries

PMIC_ON_REQ may be left unconnected, ONOFF requires pullup

as described in Table 8. Reset and ON/OFF recommendations

i.MX 8M Mini Hardware Developer’s Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,783件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi adevries

PMIC_ON_REQ may be left unconnected, ONOFF requires pullup

as described in Table 8. Reset and ON/OFF recommendations

i.MX 8M Mini Hardware Developer’s Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,782件の閲覧回数
adevries
Contributor V

Hi Igor,

Thanks for the response. I will do that. However, I think Figure 6-31 in the reference manual is a bit misleading. I interpreted it as ONOFF having an internal pull-up, but it would appear that is not the case.

pastedImage_1.png

Thanks

0 件の賞賛
返信