How to start weston without gpu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to start weston without gpu

3,943件の閲覧回数
hongxingyu1982
Contributor III

 Now I am using LCDIF->DSI->HDMI for main display on mx8mq yocto, but once I removed GPU from device tree(.dts), It seems the wayland/weston doesn't startup, and it is black screen. So how can I start wayland/weston without gpu?

Any suggestion are welcome!

0 件の賞賛
返信
3 返答(返信)

3,843件の閲覧回数
b36401
NXP Employee
NXP Employee

Here is a document regarding to Weston:
https://community.nxp.com/docs/DOC-95380
It is about i.MX6 but there is nothing very special to i.MX8.

0 件の賞賛
返信

3,843件の閲覧回数
hongxingyu1982
Contributor III

Hi Victor

Thanks you very much for your reply.

I have checked 

https://community.nxp.com/docs/DOC-95380

It seems there are two import patchs as blew:

Original Attachment has been moved to: 0002-Enable-weston-for-Vivante-GPU.patch.zip

Original Attachment has been moved to: 0001-DRM-condition.patch.zip

But It seems I can't open it. Could you support it for me?

Thanks

BR

0 件の賞賛
返信

3,843件の閲覧回数
b36401
NXP Employee
NXP Employee
0 件の賞賛
返信