How to start i.MX design ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to start i.MX design ?

1,769 次查看
Maciek
Contributor V

Hi,

We are working with 32bit microcontrollers (Kinetis, Coldfire...)

and 16/32bit DSC (like 56F84xx). So, we have no experience with

"big" processor design. Whenever we can, we use MQX OS.

I would like to investigate: how to start design based on

i.MX5 and i.MX6 devices and some available operating system. I may use

Windows Embedded Compact, Embedded Linux or Android.

What should I do first ? How about starting with some reference

platform ? How to get and use BSP for hardware platform and

operating system ?

Please advice.

Thanks for help

Maciek

标记 (3)
0 项奖励
回复
3 回复数

1,553 次查看
markvolodarskiy
Contributor I

I would suggest to start with set Mcimx53 start-R it is available completely all the background information

IMX53QSB Product Summary Page

, as well all of the source data for a quick start of the study and is the budget version

IMX53QSB Product Summary Page

1,553 次查看
Maciek
Contributor V

What about toolchain ? We are using CW Pro - but I can't see any support for i.MX architecture.

How the general workflow look like (in a few words) ?

M.

0 项奖励
回复

1,552 次查看
markvolodarskiy
Contributor I

yes it does not support Cade Warrior, you can use either iar or GCC.

http://gcc.gnu.org

Personally, I liked this board that it comes with a full Ubunta(sdcard4GB) and you can immediately see the potential of the processor was vga output.

0 项奖励
回复