How to solve the problem that the imx6dl console print the fb0 error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to solve the problem that the imx6dl console print the fb0 error

1,041 次查看
pengxingwei
Contributor III

Hello all,

            I come cross a problem ,the imx6dl console is always print the log:

[2308151.755871] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308152.265892] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308152.775892] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308153.285885] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308153.795892] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308154.306169] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308160.235880] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308160.745877] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308161.255889] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308161.765887] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308181.575883] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308182.095867] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308183.115928] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308183.635924] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308187.345912] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308187.855995] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308188.885913] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[2308189.395906] mxc_sdc_fb fb@0: timeout when waiting for flip irq

my platform is imx6dl,on which run Android6.0.1 OS (kernel 4.1.15) , the lcd display is normal ,but when the board is run for a long time about several days, the LCD display is abnormal ,and I print the log by uart console,it always print:

mxc_sdc_fb fb@0: timeout when waiting for flip irq

How to solve it ? Thanks

0 项奖励
回复
1 回复

927 次查看
joanxie
NXP TechSupport
NXP TechSupport

The error means there is display underrun on IPU. what operation do you do when the board is runing?To reduce the failure, the customer can add "dmfc=3" in the kernel boot command line

0 项奖励
回复