How to solve over-scanning problem?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to solve over-scanning problem?

ソリューションへジャンプ
5,428件の閲覧回数
Tarek
Senior Contributor I

Hi,

Part of the console display is hidden when using HDMI TV.

I guess this is due to the TV over-scanning. Is there a solution to this problem?

Thanks,

Tarek

ラベル(3)
0 件の賞賛
返信
1 解決策
4,775件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Chun-Yi Cheng wrote:

The solution for over-scanning issue was applied into i.MX Android R10.3.1 release.

The kernel patch of Android should also be able to use in Linux.

Please refer to "4.4.5 overscan" of the attached "i.MX_Android_R10.3.1_User_Guide" for more detail information.

Thanks.

  • how to apply this feature

     We export a property (sys.overscan.percent) to control the overscan percentage, customer can set this property to adjust the width of black border. (sys.overscan.percent = 100*h/H =100*w/W)  The overscan percentage for width and height is the same, sys.overscan.percent Is limited at the range of 0~10.


元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,776件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Chun-Yi Cheng wrote:

The solution for over-scanning issue was applied into i.MX Android R10.3.1 release.

The kernel patch of Android should also be able to use in Linux.

Please refer to "4.4.5 overscan" of the attached "i.MX_Android_R10.3.1_User_Guide" for more detail information.

Thanks.

  • how to apply this feature

     We export a property (sys.overscan.percent) to control the overscan percentage, customer can set this property to adjust the width of black border. (sys.overscan.percent = 100*h/H =100*w/W)  The overscan percentage for width and height is the same, sys.overscan.percent Is limited at the range of 0~10.


0 件の賞賛
返信
4,775件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

would you tell me more detail about your question?

1. which board are you using?

2. which BSP are you using?

3. how to reproduce the problem on the board?

Thanks.

0 件の賞賛
返信
4,775件の閲覧回数
Tarek
Senior Contributor I

The board I'm using is Nitrogen 6Q Board from Boundary Devices. The BSP is version 12.08 as I don't have access to 12.09 yet. I'm running Poky distribution and using Yoctoproject openembedded build system.

The board is connected to DGM HD TV using HDMI. Any Linux image that I run (Console or GUI) I find that part of the display around the edges is hidden as if I need to down size the screen to fit into the TV display. This is a common problem and surprisingly there is Android fix from Freescale

https://community.freescale.com/message/271488#271488

I was wondering if there is a similar patch for native Linux?

Thanks

0 件の賞賛
返信
4,775件の閲覧回数
fengwei
NXP Employee
NXP Employee

Usually TV has display settings for over-scanning problems.

0 件の賞賛
返信
4,775件の閲覧回数
Tarek
Senior Contributor I

It will be easier to change the platform than asking customers to change their TV's !

0 件の賞賛
返信
4,775件の閲覧回数
fengwei
NXP Employee
NXP Employee

Yes, you are right. I'm not the right person to answer this question :-). Let's wait for the golden answer.

0 件の賞賛
返信