How to shutdown and start linux on wandboard?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to shutdown and start linux on wandboard?

1,217 Views
nitigupta
Contributor I

Hi All,

Currently I am working on wandboard-quad. As my project demands, I have to shutdown and again start the linux on wandboard without actually removing power or pushing reset button. Is there any way to send signal to wandboard to shutdown linux and signal it to start linux  without removing power or pushing reset button ( may be through GPIO).

Regards,

Niti Gupta

0 Kudos
Reply
1 Reply

1,005 Views
igorpadykov
NXP Employee
NXP Employee

Hi Niti

one can check

Arch Linux ARM • View topic - [wandboard quad]reboot command does not boot [nearly solved] 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply