How to setup double monitor.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to setup double monitor.

1,083 次查看
zikoel
Contributor I

Hi,

I have a congatec board with i.MX6 processor. On it there is one monitor to HDMI adatper (with my desktop) and two more monitor (TFT 15") into LVDI interface. I am able to play video with gstreamer in both TFT monitor.

How can I setup the two display TFT as normal desktop? I want to run an application in the first and another in the second.

For now my OS is Ubuntu 11.10 with kernel 3.0.35

Thank you!!

标签 (3)
标记 (3)
0 项奖励
回复
1 回复

1,007 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

I am not familiar with congatec board, but for  i.MX6DQ SabreAI one can try

attached patch, sending the same IPU DI content to LVDS and HDMI.

IPU0 DI0 drives both LDB and HDMI.

Video parameters should be: video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24 ldb=sin0

                                          video=mxcfb1:dev=hdmi,1024x768@60,if=RGB24

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复