How to setup MCIMX8QXP-CPU Evaluation board at USB Host?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to setup MCIMX8QXP-CPU Evaluation board at USB Host?

4,357 Views
anaseem
Contributor IV

I'm booting from SD card that came with the evaluation board.  I'm booting with embedded Linux distribution that came with the board.

When I connect my usb device to USB Type C connector, does evaluation board think I connected a usb host?  

Attached are log when usb device is connected to evaluation board and when device is removed from evaluation board.

If evaluation board is setup as usb device, how can I set it up as usb host?

Tags (1)
0 Kudos
Reply
2 Replies

4,233 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Amer,

I’m afraid that i.MX8QXP family is still on preproduction, and we cannot provide additional information or support through this channel yet. In case of requiring help about i.MX8X, please directly contact with your Sales/FAE.

 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply

4,235 Views
anaseem
Contributor IV

>> When I connect my usb device to USB Type C connector, does evaluation board think I connected a usb host?

i. MX8QXP evaluation board is detecting USB devices because when I connect well know USB device, like USB Memory Stick, it gets detected. 

0 Kudos
Reply