How to setting multiple displays

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to setting multiple displays

843件の閲覧回数
Rayn_Jang
Contributor I

Hello,

Someone please help me.

We are trying to use the following dual display,

1. LVDS(LCD)

2. HDMI LVDS (LCD) displays normally.

When connecting HDMI, I want LVDS+HDMI dual display output.

The BSP and CPU information we are using is below.

BSP : Android 11.0.0_2.6.0 (Linux 5.10.72 kernel)

CPU : IMX8MP

The current problem is that if we disable the lcd (LVDS) panel driver, HDMI output is possible,

but if we enable the lcd (LVDS) panel driver, There is no HDMI output, so dual display is not possible.

I would like to know the device tree file and any additional modifications required for dual display output. Attached is our device tree file that we are using for LVDS (LCD) output.

BR,
Ryan

ラベル(1)
0 件の賞賛
返信
1 返信

802件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ryan,

I see that our engineer already give you update in the salesforce system, if you still have questions you can contact us freely.

Wish you have a nice day

Best Regards

Rita

0 件の賞賛
返信