How to set the dual display with different context in imx8mq

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set the dual display with different context in imx8mq

4,823 次查看
hongxingyu1982
Contributor III

Hi sir

Now I used the imx8mq evk board to test the dual display, one is hdmi(default), the other is mipi-to-hdmi. When I set the correct bootargs and dts files, both display can work, but with the same context when I run the demo. So If I would like to the two display the different context,  for example I would like to the mipi-to-hdmi to dispaly the demo, and the hdmi display the android home screen. How could I set? Could you give me some solutions ?

The Andriod version is :evk_8mq_eng 9 1.0.0-ga-rc3 20190114 dev-keys

Attachment is the code of demo, please check.

Thanks

0 项奖励
回复
12 回复数

4,613 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

 

According to the Android Release notes for the Android release 9.0.0_2.3. The i.MX6MQ is only able to play mirrored images in different displays(LVDS-to-HDMI+HDMI). The BSP is not capable of play different content for each screen.

 

I apologize for the inconvenience this could give you.

 

Best regards,

Diego

0 项奖励
回复

4,613 次查看
hongxingyu1982
Contributor III

Hello, Diego

Thank you very much for your reply.

But My boarad is i.MX8MQ, not 6MQ. And I see the blew, It seems i.MX8MQ can dispaly the different context.

i.MX 8MQ Dual Display Demo - YouTube 

BR.

0 项奖励
回复

4,613 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

I apologies, that was my mistake. I was referring to the i.MX8MQ instead of the i.MX6Q. Unfortunately, the dual-display with different contents is only supported by our Linux BSP. Android does not support dual-display.

If you go to the Android release notes document, Table 2, page 4. You could find that only the mirrored dual-display is supported by our Android BSP in the i.MX8MQ.

dual display support.jpg

I apologize for the inconvenience this may cause you.

Best regards,

Diego. 

0 项奖励
回复

4,613 次查看
hongxingyu1982
Contributor III

HI Diego

You could find that only the mirrored dual-display is supported by our Android BSP in the i.MX8MQ.

      ----I would like to know where set the mirrored dual-display in codes, Could you show me?

Thanks

BR

0 项奖励
回复

4,613 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

You could find more information about how is configured the mirrored display in our BSP in the fsl-imx8mq-dual-display.dtb or dtbo-imx8mq-dual.img. Unfortunately, further information related to this is more related to how the AOSP works and this out of our scope of support. I apologize for the inconvenience this could give you.

Best regards,

Diego.

0 项奖励
回复

3,942 次查看
PunitTeksun
Contributor I

Hello diegoadrian,

Can you please confirm if the IMX8QM supports the DIffernt context on the different display? 

our both the displays are up and running and we are getting mirrored screen. can you please let us know where to check to disabled the mirroring. 

0 项奖励
回复

4,613 次查看
hongxingyu1982
Contributor III

Hi Diego

If I would like to the dual-display with different contents with Android, I should changed the Android surfaceflinger or APP codes, is it right ?

BR

0 项奖励
回复

4,613 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Probably it could be at the APP code level. I found the following information. However, this is out of our scope off support. We cannot guarantee anything. I apologize for the inconvenience this could give you.

Presentation  |  Android Developers 

Best regards,

Diego.

0 项奖励
回复

4,613 次查看
hongxingyu1982
Contributor III

Hi Diego

I see there is a apk HdmiDualVideo can setting the different context with dual dispaly in

iTOP-iMX6 board, as blew:

hdmi_dual_video.png

But It seems there is no this apk for imx8mq, why ?

Br

0 项奖励
回复

4,613 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

The iTOP-iMX6 is a board from a third-party. For specific support of that application, I suggest you go with them. I apologize for the inconvenience this could give you.

Best regards,

Diego.

0 项奖励
回复

4,613 次查看
hongxingyu1982
Contributor III

Hi everyone

Is there anyone can help to solve this issue ?

BR

0 项奖励
回复

4,063 次查看
JoergAlbert
Contributor I

Hi,

 

did you make any progress on this issue?

I have a similar problem. Got a 8MPLUSLPD4-EVK with the NXP Android 13 BSP and the release notes still say "mirrored display". But we want to display different content on three displays connected via HDMI and LVDS.

Regards,

Joerg

 

0 项奖励
回复