Hi community,
I have some questions about i.MX6DL IPU setting.
[Q1]
Please see Figure 38-45 in IMX6SDLRM Rev.1.
I understand I can set "Display height (lines)" by DIx_SCREEN_HEIGHT field in IPU_DIx_SCR_CONF register.
Is my understanding correct?
[Q2]
How can I set "Display width (pixels or accesses)"?
[Q3]
I understand antive wildow resolution and LCD resolution are not necessarily the same.
If the LCD resolution is 1920 x 1080, I have to set "Display width (pixels or accesses)" = 1920 and "Display height (lines)" = 1080.
But I can set AW_HEND <= 1920 and AW_VEND <= 1080.
Is this correct?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
The IPU DI provides display sync signals, corresponding waveforms,
where screen size parameters are (in some sense) “hardcoded” via DC microcodes
IPU_DIx_SCR_CONF register also should be set.
This is possible to configure active window size parameters less than actual
 display sizes.
The IPU DI provides display sync signals, corresponding waveforms,
where screen size parameters are (in some sense) “hardcoded” via DC microcodes
IPU_DIx_SCR_CONF register also should be set.
This is possible to configure active window size parameters less than actual
 display sizes.
Dear Yuri,
I have a question for LCD configuration.
I can see the LCD Configuration values in include/linux/fb.h like as below,
<Linux>/include/linux/fb.h
struct fb_videomode { <CLAA-WVGA>
const char *name; /* optional */ : "CLAA-WVGA" : CLAA-WVGA :
u32 refresh; /* optional */ : 57 : Refresh rate in Hz : FV
u32 xres; : 800 : resolution in x : HDISP
u32 yres; : 480 : resolution in y : VDISP
u32 pixclock; : 37037 : Pixel clock in picoseconds :
u32 left_margin; : 40 : Horizontal Back Porch : HBP
u32 right_margin; : 60 : Horizontal Front Porch : HFP
u32 upper_margin; : 10 : Vertical Back Porch : VBP
u32 lower_margin; : 10 : Vertical Front Porch : VFP
u32 hsync_len; : 20 : Hsync pulse width :
u32 vsync_len; : 10 : Vsync pulse width :
u32 sync; : FB_SYNC_CLK_LAT_FALL : Polarity on the Data Enable :
u32 vmode; : FB_VMODE_NONINTERLACED : Video Mode :
u32 flag; : 0 : 0 :
};
Could you tell me what register was configured for each values of fb_videomode?
Best Regards,
Eric.
Linux documentation for i.MX6 does not contain recommendations for LCD using / adaptation.
I think we can use Chapter 18 (Supporting the i.MX53 Reference Board DISP0 LCD) of
i.MX53 System Development User’s Guide to clarify some aspects for i.MX6 too.
http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf