How to set correct clock-frequency in MIPI DSI Display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set correct clock-frequency in MIPI DSI Display

3,672 次查看
cs_lin
Contributor II

hi, 

now we are porting Tianma TM050JDHC02 panel into imx8mq custom board. with vendor provided panel config as below, 

#define LCM_PCLK 82
#define LCM_HACT 720
#define LCM_HFP 92
#define LCM_HBP 80
#define LCM_HSA 20
#define LCM_VACT 1280
#define LCM_VFP 200
#define LCM_VBP 16
#define LCM_VSA 2
#define LCM_NLANE 4
#define LCM_VDOMODE 0
#define LCM_MIPISPEED 500

Our question is, if we set LCM_PCLK to 82Mhz or 120Mhz to "clock-frequency" in DTS (please refer to DTS.txt), then panel will show nothing, and you will have a of of 

[ 1.474487] [drm] Cannot find any crtc or sizes
[ 1.479995] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0

you can refer the log of log inilog_82Mhz.log for full logs.

But if we set it to 132MHz, we it can show the display content, but if will have a log of

dcss-core 32e00000.dcss: Pixel clock set to 120000 kHz instead of 132000 kHz, difference is -12000000 Hz (inilog_132Mhz.log)

Can you help figure out what's wrong with clock-frequency setting in DTS? and what should we modify in DTS to have LCM_PCLK as 82Mhz?

thank you!

标记 (1)
0 项奖励
回复
1 回复

3,270 次查看
igorpadykov
NXP Employee
NXP Employee

Hi CS Lin

there are some limitations on clock, for example one can check valid_clocks[] in

nwl-dsi.c\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

Recommended to try latest L4.19.35 kernel or workarounds described on

https://community.nxp.com/thread/513899 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复