Hi All!
I'm working on an iMX23 cpu with linux-2.6.35.3 and wondering if this is even possible to implement.
I can build g_serial and g_multi and use the serial port function, which uses /dev/ttyGS0.
Do I just have to change [console=ttyS0] to [console=ttyGS0] on the kernel command line?
Thanks
已解决! 转到解答。
I added another console setting in [/etc/inittab]
::respawn:/sbin/getty -L ttyAM0 115200 vt100
It works fine!