How to set TAMPER pins as GPIO whose properties are equal to device tree.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set TAMPER pins as GPIO whose properties are equal to device tree.

5,592 次查看
Hirotoshi_Sato
Contributor II

Hi, I am confused how can I set TAMPER pins as GPIO whose properties are equal to device tree.

I use imx6ull board.

I directly accessed register address with memtool and got following information.

SW_MUX_CTL_PAD_SNVS_TAMPER1: reg val 0x0

SW_PAD_CTL_PAD_SNVS_TAMPER1: reg val 0x0

other tamper pins are the same as above.

However I defined these pins for GPIO in device tree as follows.

&iomuxc {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_hog_1>;
imx6ul-evk {
pinctrl_hog_1: hoggrp-1 {
fsl,pins = <

MX6UL_PAD_SNVS_TAMPER1__GPIO5_IO01 0x000110B0
MX6UL_PAD_SNVS_TAMPER3__GPIO5_IO03 0x0000B0A0
MX6UL_PAD_SNVS_TAMPER5__GPIO5_IO05 0x000110B0
MX6UL_PAD_SNVS_TAMPER7__GPIO5_IO07 0x000110B0
MX6UL_PAD_SNVS_TAMPER8__GPIO5_IO08 0x000110B0
MX6UL_PAD_SNVS_TAMPER9__GPIO5_IO09 0x000110B0

The values of device tree do not set in the register.

The IMX6ULRM says that TAMPER_PIN_DISABLE in fuse has to be 11 to disable TAMPER0-9 and use as GPIO.

So I checked 0x430[21:20] and got 11. I think this means tamper pins are set as ALT5 GPIO mode.

I checked fuse in uboot too (refer to mx6ul tamper pin to gpio  ). The result is following.

Hit any key to stop autoboot: 0
=> fuse read 0 3
Reading bank 0:

Word 0x00000003: 71300070

note that 0x71300070 = 1110001001100000000000001110000

From the beggining, TAMPER_PIN_DISABLE is 11. Can I set them in device tree? I could not find any definition of tamper pins.

I could export these tamper pins in sysfs, but the values cannot be written even if I set them as output direction.

The values are always HIGH.

Why can't I set register values as defined in device tree ?

Why can't I change H/L even if I set tamper pins as output direction?

标签 (4)
0 项奖励
回复
4 回复数

4,001 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hirotoshi

please look at imx6ull-14x14-evk.dts example, using &iomuxc_snvs..

linux-imx.git - i.MX Linux Kernel 

in latest Linux 4.9.11_1.0.0 BSP, description on link

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,001 次查看
Hirotoshi_Sato
Contributor II

Thank you for your reply.

I found that I defined MX6UL_PAD_SNVS_TAMPER1__GPIO5_IO01 0x000110B0 though I use imx6ULL.

So I defined in imx6ull-var-dart.dtsi as follows and removed the description of  MX6UL_PAD_SNVS_TAMPER...

&iomuxc_snvs {
pinctrl-names = "default_snvs";
pinctrl-0 = <&pinctrl_hog_2>;
imx6ul-evk {
pinctrl_hog_2: hoggrp-2 {
fsl,pins = <
MX6ULL_PAD_SNVS_TAMPER1__GPIO5_IO01 0x000110B0
MX6ULL_PAD_SNVS_TAMPER3__GPIO5_IO03 0x0000B0A0
MX6ULL_PAD_SNVS_TAMPER5__GPIO5_IO05 0x000110B0
MX6ULL_PAD_SNVS_TAMPER7__GPIO5_IO07 0x000110B0
MX6ULL_PAD_SNVS_TAMPER8__GPIO5_IO08 0x000110B0
MX6ULL_PAD_SNVS_TAMPER9__GPIO5_IO09 0x000110B0
>;
};
};
};

It seems to work as GPIO because H/L can be changed by sysfs.

Next, I would like to check the register value.

iomuxc_snvs is defined as follows:

iomuxc_snvs: iomuxc-snvs@02290000 {
compatible = "fsl,imx6ull-iomuxc-snvs";
reg = <0x02290000 0x10000>;
};

So the base address is 0x2290000.

/*
* The pin function ID is a tuple of
* <mux_reg conf_reg input_reg mux_mode input_val>
*/
#define MX6ULL_PAD_BOOT_MODE0__GPIO5_IO10 0x0000 0x0044 0x0000 0x5 0x0
#define MX6ULL_PAD_BOOT_MODE1__GPIO5_IO11 0x0004 0x0048 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER0__GPIO5_IO00 0x0008 0x004C 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER1__GPIO5_IO01 0x000C 0x0050 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER2__GPIO5_IO02 0x0010 0x0054 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER3__GPIO5_IO03 0x0014 0x0058 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER4__GPIO5_IO04 0x0018 0x005C 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER5__GPIO5_IO05 0x001C 0x0060 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER6__GPIO5_IO06 0x0020 0x0064 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER7__GPIO5_IO07 0x0024 0x0068 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER8__GPIO5_IO08 0x0028 0x006C 0x0000 0x5 0x0
#define MX6ULL_PAD_SNVS_TAMPER9__GPIO5_IO09 0x002C 0x0070 0x0000 0x5 0x0

From above, MX6ULL_PAD_SNVS_TAMPER1 address is 0x2290000 + 0x000C = 0x229000C.

So I checked with /unit_tests/memtool. However I could not access the register.

The result is 

root@imx6ul-var-dart:/unit_tests# ./memtool 229000c 1
E
Reading 0x1 count starting at addUnhandled fault: external abort on non-linefetch (0x1008) at 0x76faf00c
pgd = 885d0000
[76faf00c] *pgd=885f4831, *pte=02290703, *ppte=02290e33
ress 0x0229000C

Bus error

What is the problem? The addrss I accessed is wrong?

What is the register address of imx6ull not imx6ul?

4,001 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hirotoshi

for addresses please check Chapter 33 IOMUX Controller (IOMUXC)
i.MX6ULL Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf

Best regards
igor

0 项奖励
回复

4,001 次查看
joseluiszabalza
Contributor II

Hello igor

I have the same problem and i don't understand the answer.

Why memtool can't access to 229000c address?