How to set NAND_READ_CMD_CODE1/2 for NAND Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set NAND_READ_CMD_CODE1/2 for NAND Boot

879 次查看
MartinHo
Contributor IV

Hi I'm working on the fuse configuration to boot from my raw NAND (MT29F4G08ABAEA), but I'm confused if I have to set the two NAND_READ_CMD_CODE fields. Do I need to burn this fuses and if Yes to what value (Read Page --> 0x00 and 0x30 ?). 

I have already set the following fuses: 

0x05 (b00,w05) 0x0450 OCOTP_CFG4           = 0x00001280 

   CFG1 = NAND, raw, 1 Device, 3 row address bytes (nedds to be 5 row?)

   CFG2 = Block has 64 Pages, BOOT_SEARCH_CONT = 4

   CFG3 = not used

   CFG4 = not used

0x06 (b00,w06) 0x0460 OCOTP_CFG5           = 0x00000010

(BT_FUSE_SEL = 1)

Con You please help me to set

0x07 (b00,w07) 0x0470 OCOTP_CFG6   

thanks

Martin

标签 (1)
0 项奖励
回复
1 回复

781 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

nand boot will work fine without changing default NAND_READ_CMD_CODE fields.

They can be used for some non-standard cases.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复