How to set GPIO state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set GPIO state

ソリューションへジャンプ
3,481件の閲覧回数
xu_ji1
Contributor V

Hi,

About Yocto project,how to set the GPIO high when system boot on

Please give guide

Thanks

タグ(1)
0 件の賞賛
返信
1 解決策
3,195件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can look at Porting Guide included in Linux L4.14.98_2.0.0 Documentation

dts example of gpio : pinctrl_pcieb to control PCIe :

fsl-imx8qxp-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,195件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xu

one can try to set it using scfw, please check

SCFW Porting Kit

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,194件の閲覧回数
xu_ji1
Contributor V

Sorry,

I don't want to changed in SCFW ,I want to set it in boot and kernel,it is better in dts

Thanks

0 件の賞賛
返信
3,196件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can look at Porting Guide included in Linux L4.14.98_2.0.0 Documentation

dts example of gpio : pinctrl_pcieb to control PCIe :

fsl-imx8qxp-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor

0 件の賞賛
返信