My configure below.
Linux kernel 3.0.35
OS Ubuntu 12.04
I.mx6dl Board
------------------------------------------------------------------------------------------
Hi everyone.
In my case, not use camera. just use csi0 driver(mxc_v4l2_capture) and ov5640 camera driver and app.
ov5640 driver set image is below
ov5640_mode_VGA_640_480 | |
ov5640_mode_QVGA_320_240 | |
ov5640_mode_NTSC_720_480 | |
ov5640_mode_PAL_720_576 | |
ov5640_mode_720P_1280_720 | |
ov5640_mode_1080P_1920_1080 | |
ov5640_mode_QSXGA_2592_1944 | |
ov5640_mode_QCIF_176_144 | |
ov5640_mode_XGA_1024_768 |
If i want to add size 6144 X 3072 , how to change code?
According to the manual(IMX6SDLRM : 2818p, 2877p ) that can
change elements (sensor frame width (height)and active frame width(height) and clock(F=FH*FW*FPS*BI*DF) )
I don't know. what files are check .I already check like that mxc_v4l2_capture.c(in kernel) , ov5640.c(in kernel), ,ipu_capture.c ,ipu_regs.h(in linux/ipu3) ..
How to check and modify correct files?
Solved! Go to Solution.
Please refer to the Chapter 7 of the attached document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The document is attached to my previous post. I'm attaching it once again. Also, this i.MX6Solo/DualLite BSP Porting Guide document can be found as the part of the L3.0.35 BSP Documentation package, available for download on the NXP web site:
Best Regards,
Artur
Please refer to the Chapter 7 of the attached document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur.
Thank you for your reply.
By the way, where is the attached document?
Have a nice day~!