How to run the sdk_unit_test ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run the sdk_unit_test ?

ソリューションへジャンプ
1,473件の閲覧回数
patcharasirigul
Contributor II

Hello everyone,

     I downloaded the i.MX 6Series Platform SDK. I'd like to know how to run all_test.c or unit_test_main.c for testing the SABRE-SD Board.

Thank you,

ラベル(3)
0 件の賞賛
返信
1 解決策
1,383件の閲覧回数
saurabh206
Senior Contributor III

Hi,

You can refer iMX6_Platform_SDK\doc

Which provides all the information.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,383件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please take a look at README.pdf file in the SDK package.

Also, to build the tests, Linux host is preferable.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,384件の閲覧回数
saurabh206
Senior Contributor III

Hi,

You can refer iMX6_Platform_SDK\doc

Which provides all the information.

0 件の賞賛
返信