How to run at 1.5GHz for MCIMX8M-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run at 1.5GHz for MCIMX8M-EVK

1,094 Views
ko-hey
Senior Contributor II

Hi all

 

Q1.

According to the line 28 in attachment, it seems that the CPU is running at 1000MHz.

Is it true ?

 

Q2.

I want to evaluate it at 1500MHz.

Is there any demo image for 1500MHz ?

 

Q3.

If there are no demo image for 1500MHz, could you tell me how to run at 1.5GHz for MCIMX8M-EVK ?

 

 

Ko-hey

 

0 Kudos
Reply
1 Reply

991 Views
b36401
NXP Employee
NXP Employee

You can manage CPU frequency with sysfs. I mean /sys/devices/system/cpu/cpu0/cpufreq structure.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply